10/10/2022 7:39 AM | |
Joined: 1/11/2019 Last visit: 9/10/2024 Posts: 758 Rating:
|
Hello Borudek, Configuration: Use the CFC editor to install the block in a cyclic interrupt OB (OB30 toOB38). The block is also installed automatically in the startup OB (OB100). When the CFC function "Generate module drivers" is used, the following occurs automatically:
In case of redundancy, connection with both quality bits and connection with the redundant slave channel:
Connect the symbol generated in HW Config (symbol table) for the output channel with thePV_Out output parameter. In case of redundant I/O configuration, use symbol of the channel of the master module. The templates of the Advanced Process Library contain an example of anPcs7DiOu application. |
7/10/2023 9:10 AM | |
Joined: 10/16/2020 Last visit: 4/13/2024 Posts: 1 Rating:
|
Hi I have the same problem, did you manage to solve it |
7/29/2023 3:49 AM | |
Joined: 1/11/2019 Last visit: 9/10/2024 Posts: 758 Rating:
|
Hello, Please try the given solutions and post the feedback |
7/31/2023 6:52 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hi AutoGen_8390654, I assume that you use I/O modules which are released for PCS 7 or? All other I/O modules wouldn't work with the automatically driver generation. The released I/O modules for PCS 7 can be found in the manual PCS 7 Released modules (V9.1 SP2). Which catalog did you use to configure the I/O modules? Did you use the "Standard" catalog or the "PCS 7" catalog? If you configure the I/O module from the "Standard" catalog and it is released for PCS 7 also the automatically driver generation wouldn't work. Please make sure that the I/O module in the HW-Config is from the PCS 7 catalog. With regards |
5/29/2024 11:55 AM | |
Joined: 1/11/2019 Last visit: 9/10/2024 Posts: 758 Rating:
|
Is it! Then, Please raise an service request for the same. and post the solution later. Use the below link to raise a request. Create Service Request |
Follow us on