12/7/2023 8:33 AM | |
Joined: 10/5/2023 Last visit: 5/29/2024 Posts: 4 Rating: (1) |
Hello For my project, I need to control a stepper motor with a Siemens s7-1200 DC/DC/DC PLC and a STR-2M stepper motor driver. But when I follow the wiring advice, it doesn't work. 24V for3L GND fot 3M PWM on .0 Direction on .1 and enable on .2 The only way I found is to put PWM signals in COM+ and GND in STEP but with this wiring I can't use direction and enable. Do you have a suggestion? Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/08/2023 07:35:45New subject after splitting |
|
1/9/2024 3:26 PM | |
Joined: 10/5/2023 Last visit: 5/29/2024 Posts: 4 Rating: (1) |
thank you very much for your help. it works
|
This contribution was helpful to1 thankful Users |
Follow us on