8/5/2024 5:06 PM | |
Joined: 9/28/2016 Last visit: 8/13/2024 Posts: 6 Rating:
|
I have a continuous issue whenever I try and download parameters to (seems like) any Simovert Masterdrives Compact Plus unit. Here is what happens: I connect to Drive Monitor and use the "save drive parameters to file" button to save to my computer. However, even without changing a single thing at that point, if I THEN go to "download parameter file to drive", I almost always get a whole slew of errors during the process. Then when it asks if I'd like to retry, I'll do it again, and the same thing will happen, and the number of errors will change. Sometimes, if I do it a second or third time, it will just go through with zero errors. Sometimes it will just keep going in this cycle and never end. Sometimes I'll get an unrecognized device error. Throughout the process, I will keep seeing the "Device Identification" box pop up, and it seems like at this moment is when the errors start racking up. What is causing this with every single drive? I had asked something similar to this years ago and was told to make sure P070 matches the model number, but it always does, and this still happens. Attachmentattatchment.pdf (62 Downloads) |
Last edited by: Waldo924 at: 08/05/2024 17:10:09Last edited by: Waldo924 at: 08/05/2024 17:30:33Last edited by: Moderator_Lan at: 08/06/2024 07:48:05Files attached as pdf Last edited by: Waldo924 at: 08/06/2024 21:06:59 |
|
Follow us on