7/26/2024 9:32 AM | |
Joined: 8/3/2009 Last visit: 9/27/2024 Posts: 13803 Rating: (1741)
|
Hello Colin Malcolm you cannot switch only the SQL Server Version. If you need WinCC flexible 2008 SP3 you have to get sure first if you Operating System is compatible with WinCC Flexible 2008 SP3 -> because Win10 or newer is NOT released and compatible with SP3! (only with SP5) LINK So if this fits, you would have to uninstall WinCC Flexible complete and als the SQL Server of this System and then you can install 2008 SP3 (its because this version is only released with specific SQL Version -> check in Compatool) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on