3/6/2024 9:16 AM | |
Posts: 1 Rating:
|
Hi, im trying to connect SiWare to my Controlatron 1020N model FST020 by RS232 to usb cable using manual provided i nead to get communication by COM1 but the program is only giving me two ways TCP&IP and COM3. I use COM3, then go to connection open the connection menue click OK then the i get "Cannot Open Comm Port - Error Code:5 " can you help me with this ? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/07/2024 11:52:07New subject after splitting |
|
Follow us on