3/6/2015 2:51 PM | |
Posts: 2 Rating:
|
Hi, At the moment I'm making an application where a little wheel is drived by a dc - motor. When I send out the wheel at maxed velocity (int value 27648) i can't measure the wheel anymore with a normal counter. I'm measuring it by counting the times the inductive sensor gives me a value = true. I want to try the HSC but i do not know what parameter is the input signal. To be complete: i'm working with a S7-1215 DC/DC/DC CPU and i'm programming in SCL. I hope u can help me. Kind regards |
10/27/2015 8:21 PM | |
Posts: 1 Rating:
|
Gracias x la informacion, me sirvio (Y) |
3/10/2016 10:36 AM | |
Posts: 1 Rating:
|
dear sir I cant open HSC.zip (example) ?? please i need it , if you can send me the zip again ?? thanks a lot |
4/9/2017 5:08 PM | |
Joined: 3/18/2010 Last visit: 7/21/2025 Posts: 3 Rating:
|
Very usefull explanation, as usual Denilson. Thanks
|
5/12/2017 2:36 AM | |
Joined: 4/26/2017 Last visit: 6/23/2025 Posts: 74 Rating:
|
Dear Denilson, do you can rewrite this code to open it on Tia Portal V14? |
8/24/2017 1:15 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, AttachmentHSC_V14.zip (1165 Downloads) |
Denilson Pegaia |
|
Follow us on