1/31/2022 3:12 PM | |
Joined: 9/27/2006 Last visit: 11/11/2024 Posts: 12293 Rating: (2691)
|
Hello qwemx; There are few passive "listener" staions offered in the market for Profibus-DP, some process value displays acting as listeners on Profibus-PA are available, for examle these units from BEKA (note, no OPC connection): https://www.beka.co.uk/pdfs/profibus_summary.pdf The way Profibus-DP was designed makes it difficult to have listener nodes, since normally the slave nodes on the network must be connected to a master that holds a specific configuration for each one. And the use of a Class-2 master (HMI, SCADA station), even thugh it requires no configuration in the Class-1 master (the PLC) still implies a node address for the HMI and changes in the Profibus token-passing. The additional OPC server functionalities you desire for your Profibus-DP listener increases the difficulty in suggesting a model, but this hardware/software combination from Softing might fit your requirements (I have no idea of pricing, though, contact Softing): hardware "listener" station not requiring a Profibus address or configuration, softwre for collecting the data from the listener and able to connect through OPC UA to remote stations. - Softing TH LINK Profibus (passive hardware Profibus station) https://industrial.softing.com/uploads/softing_downloads/TH_LINK_PB_I_EN_01.pdf - Softing TH Scope software (with OPC UA server functionalities) https://industrial.softing.com/uploads/softing_downloads/TH_SCOPE_U_V3_70-1_EN.pdf Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 01/31/2022 15:16:11Last edited by: dchartier at: 01/31/2022 16:22:24 |
|
2/23/2022 6:38 AM | |
Joined: 10/7/2005 Last visit: 11/11/2024 Posts: 3026 Rating: (1057)
|
Hi qwemx I suggest you have a look at www.iba-ag.com as an ibaPDA system in combination with an ibaBM-DP will give you exactly the capability you want. The BM-DP can be used as passive listener (or "Sniffer" as we call it, no node address required) on the PROFIBUS, read out any and all I/O data from it in real time and then push it up to the ibaPDA PC via fiber optic. Better still, the ibaBM-DP also has bus monitoring capabilities that can be used to keep a watchful eye on the long term health of the PROFIBUS Network. An OPC DA Server (as well as Client interface) is included in the PDA Server, an OPC UA Server or Client can be added via license addition if required. Should this interest you, get in touch with your local iba Office (see https://www.iba-ag.com/en/contact) and they'll look after you. |
Last edited by: fritz at: 02/23/2022 06:40:07Cheers |
|
This contribution was helpful to2 thankful Users |
Follow us on