2/28/2022 11:13 AM | |
Joined: 5/10/2015 Last visit: 8/17/2024 Posts: 3 Rating: (0) |
Hi, I am using TIA V15.1 update 6. It is not showing AI energy module 6ES7134-6PA01-0BU0 in hardware catalog of ET200SP CPU. Please help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/28/2022 12:07:41New subject after splitting |
|
2/28/2022 12:27 PM | |
Joined: 4/24/2006 Last visit: 10/8/2024 Posts: 8745 Rating: (1168)
|
Hello, Please have a look at the following link: Delivery Release: Generation change for ET200SP Energy Meter Modules of the Standard function class When you want to use TIA Portal v15.1 you will need GSD or GSDML file. Best regards, Wizard |
2/28/2022 2:09 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi royle, The module is included in TIA STEP 7 V16 or higher with HSP, otherwise you can project it over GSD file. see the technical data. There is also a note for Cross compatibility and function comparison ST/HF in the delivery release that may help you. regards, |
FCK WAR! |
|
3/2/2022 11:44 AM | |
Joined: 4/24/2006 Last visit: 10/8/2024 Posts: 8745 Rating: (1168)
|
Hello, Here you can download GSD file: PROFINET GSD files: I/O - ET 200SP Best regards, Wizard |
Follow us on