4/27/2022 3:44 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (135) |
Hello anthony dulimba, I recommend deleting the instance DB in the SIMATIC Manager and also in the CPU and creating it again in S7-GRAPH. Then repeat the download. Also do the consistency check in STEP 7. For more information, see the FAQs: How do you perform a block-consistency check following changes in the STEP 7 program? Why doesn't the sequencer switch on in automatic mode even though the transition condition is fulfilled? With best regards |
Follow us on