Industry Online Support
Technical Forum
5/30/2006 10:55 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi Zhao, Have you read the handbook of the FM352-5? You can find this handbook by Siemens on the support sides behind the link: http://support.automation.siemens.com/WW/view/en/9240171 The module is working to the standard S7-program over a I/O-interface, this is described in the handbook. A simulation of this module is so far i know not possible. [:(] But what you can do is reading what the module have for instructions inside and then make a program in STEP7 to simulate it with PLCSIM. [:P] Because a FM352-5 is very fast with his FPA-logic it is only important to check the code. If you have the module there is a possibility to look in the simulate mode to the code. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on