7/24/2023 8:26 AM | |
Joined: 10/30/2022 Last visit: 12/13/2023 Posts: 1 Rating:
|
Good morning everyone, I have a similar problem the INTERFACE MODULE IM ET200SP is blinking green on RN LED, while all the I/O are blinking green on the DIAG. Also the network ports shows indication of connection to the devices they are connected to. I checked online on the module information and it shows that the modules are configured but not available and these affects all the network devices including the frequency drive. The problem is yet to be resolved also, I need help on what could be the possible problem. I have changed both the interface module and the port adaptor module the problem remains the same. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/25/2023 09:23:39New subject after splitting |
|
Follow us on