9/12/2023 2:02 PM | |
Joined: 10/31/2005 Last visit: 4/22/2025 Posts: 366 Rating:
|
Hello, I need to create a GSDML file for SINAMICS S120 CU320. I have classic STEP 7 v5.6 project with these drives with the following details: Device family: SINAMICS I have tried to use STARTE script to generate GSDML file according to the instructs presented in teh manual "Generating_GSDML_files_for_SINAMICS_drives_V2_2_EN". The real problem is that I don't have access to the actual drives any more, and for creating the GSDML files, I need to specify original GSD files. I tried to use the following files: https://support.industry.siemens.com/cs/kz/en/view/49217480 but it's not working since the firmware version is v4.6. So, is it possible to find original GSDML files for firmware version v4.4? I test this by trying to install GSD support files in TIA v17, and there I get error messages when try to install newly created GSDML files usng scripts. Alternative would be to create these drives manually in TIA, but then I would have to reconfigure them. Is it possible to use STARTER to save configuration and then to use this saved configuration to newly created files in TIA? |
Last edited by: Jen_Moderator at: 09/13/2023 07:57:22Link optimized. |
|
Follow us on