2/24/2024 7:26 PM | |
Joined: 10/5/2023 Last visit: 5/29/2024 Posts: 9 Rating: (0) |
How to read the Current Value of Encoder in HMI? Hi there, I have set up a program on PLC1212C to execute the cutting of customized material that moves on the conveyor. In the initial settings section, I have specified these stages for the operator. Procedure for initial setup of the machine and obtaining the conveyor speed for calculating the dimensions of the material:
I want the operator to view the pulse count recorded by the encoder in the "Current Value of Encoder" field and enter it into the "Reference Encoder" field. Question: Which terminal of CTRL_HSD should the "Current Value of Encoder" field be connected to to display its encoder value? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/28/2024 11:29:46New subject after splitting |
|
2/28/2024 11:30 AM | |
Joined: 8/21/2014 Last visit: 7/29/2024 Posts: 1012 Rating: (13) |
Closed cause question posted twice. The second thread with the subject How to read the Current Value of Encoder in HMI? is published within the conference SIMATIC Technology Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on