3/21/2024 10:39 AM | |
Joined: 8/3/2009 Last visit: 6/14/2024 Posts: 13030 Rating: (1660)
|
Hello 千树华 which WinCC Version do you use ? I would say Winndows 10 Home is not released with WinCC V7/8: https://support.industry.siemens.com/cs/ww/en/view/64847781 (you should be abel to open the local user management in computer management, I´m not sure if it is the same in WinHome as in WinProf/Enterprise) Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/22/2024 12:41 AM | |
Joined: 2/28/2018 Last visit: 3/22/2024 Posts: 3 Rating: (0) |
The server system is windows server 2012 r2 64bit, running wincc 7.4 sp1. The client pc cant open the local user management due to the home edition. |
Follow us on