3/23/2024 5:21 AM | |
Joined: 1/13/2024 Last visit: 4/23/2024 Posts: 10 Rating: (0) |
Hello Dears I want to control a pump by a temperature sensor and a pressure sensor at the same time. In fact, for example, the temperature set point is 50 degrees Celsius and the pressure set point is 120 bar. How can I control the device? I have given output PID_temp to inlet PID_compact but my pressure set point always keeps the pump on its set point ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/25/2024 10:33:54New subject after splitting. Text formatting optimized. |
|
3/25/2024 10:37 AM | |
Joined: 6/19/2017 Last visit: 6/27/2024 Posts: 8204 Rating: (169) |
Closed cause question posted twice. The second thread with the subject Pump pid control by pressure and temperature is published within the conference SIMATIC Technology. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on