6/6/2024 2:24 PM | |
Joined: 7/19/2022 Last visit: 9/6/2024 Posts: 2 Rating: (0) |
Hello, I need to set up a telegram to communicate with a PLC, all in TIA portal version 17. One inverter with version G120 FV 4.7.10 has this parameter p60022 and the communication works perfectly.The other G120 FV 4.4 and 4.5 inverters have the Profisafe function turned on, but the p60022 parameter is missing, it still gives me error F01653 - 231 when trying to connect to the PLC.I see in the summary table that Profisafe telegram is not selected.I do not know what to do. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/07/2024 06:08:01New subject after splitting |
|
6/6/2024 2:24 PM | |
Joined: 7/19/2022 Last visit: 9/6/2024 Posts: 2 Rating: (0) |
|
6/7/2024 2:29 PM | |
Joined: 9/21/2012 Last visit: 9/12/2024 Posts: 4131 Rating: (463) |
In the VFD hardware config, select Telegram 30 in the Telegram config. |
Follow us on