6/17/2024 8:01 AM | |
Joined: 1/4/2013 Last visit: 10/12/2024 Posts: 1127 Rating: (102) |
Hello, to me it's not very clear why he wants an empty memory card. Anyway be VERY careful since you have a D425 and not a D425-2 According to manual , page 291, your CF card must not exceed the 1 gb memory (512 mb/1 gb cards will be ok). Technically you can bring ANY Siemens Compact flash card <= 1Gb and reprogram it with the correct Boot Sectors and, of course, with the correct firmware that was used for the D425 (4.0/4.1/4.2/ecc) Then you can do what you want. Otherwise you will insert your card and all leds will become orange, showing that that CF card was not correctly programmed. |
Searching for Siemens used/new equipments ? |
|
6/17/2024 8:19 AM | |
Joined: 7/24/2023 Last visit: 6/19/2024 Posts: 3 Rating: (0) |
thanks for the answer what exactly is the custom code because so far I have only found SINUMERIK CompactFlash card and here there are only 2GB and 8
|
6/17/2024 8:50 AM | |
Joined: 1/4/2013 Last visit: 10/12/2024 Posts: 1127 Rating: (102) |
Hello, code is : 6AU1400-2PA02-0AA0 Siemens specs are : https://mall.industry.siemens.com/mall/it/it/Catalog/Product/6AU1400-2PA02-0AA0 And that's the last available CF card that is compatible with D4x5 old family If you have a >1 gb CF , then it will not work with D425. You can try, but manual says it won't work
|
Searching for Siemens used/new equipments ? |
|
6/17/2024 9:39 AM | |
Joined: 7/24/2023 Last visit: 6/19/2024 Posts: 3 Rating: (0) |
they have one, but they want an empty one, because the equipment is old and it’s not clear which version will work correctly
|
Follow us on