7/10/2024 7:46 PM | |
Joined: 7/7/2010 Last visit: 10/18/2024 Posts: 15327 Rating: (2432)
|
Sounds like you need some logic to sit between the recipe screen and recipe data and dynamically translate it to/from boolean and string (text). With a comfort panel, you have many tools at your disposal. TruE and fAlSe That is likely going to create problems. Have you reviewed all references on this page: Build my own data record (Recipe) drop down list - 236442 - Industry Support Siemens
|
science guy |
|
This contribution was helpful to1 thankful Users |
8/9/2024 9:55 AM | |
Joined: 11/7/2016 Last visit: 10/11/2024 Posts: 5 Rating: (0) |
Thank you also. The idea was exactly to avoid the user input by writing or interpretation, so the user could only choose "Yes" or "No" in his own language and nothing else. Now I have to write the recipe value name as "Prewelding (0=no and 1=yes) and have te user choose 0 or 1. It would be easier if the user would have dropdown menu presented to him when he clicks the recipe data value field, ant the would only be the Yes/No options.
|
Follow us on