6/3/2022 9:20 AM | |
Joined: 5/24/2022 Last visit: 6/3/2022 Posts: 1 Rating: (0) |
I have the same problem, on both computers "Allow remote connections" is enabled and Forbid license key transfer from the local computer is disabled. still cannot connect. I get the same error: the computer is not accessible. I can ping the IP address of the destination server, which I want to copy the license there. I also tried to copy the DNS of the destination server on my computer. have someone any idea to help me? I use VPN to connect to destination sever, which IP address should I use? the both computer should connect to internet? ------------------------------------------------------------------------------------------ |
Last edited by: mehrnaz_frz at: 06/03/2022 09:22:34Last edited by: Jen_Moderator at: 06/03/2022 11:23:43New subject after splitting Last edited by: mehrnaz_frz at: 06/03/2022 13:11:13 |
|
Follow us on