5/11/2016 12:45 PM | |
Joined: 3/14/2008 Last visit: 8/3/2024 Posts: 2079 Rating: (931)
|
Hello amyLow, The logfile shows that you have not configured the target path correctly. I can see you used an IP address instead of the computername in your target OS assignment. I'm not familiar by using IP addresses.. So, please fill in the computername instead of the IP address and try again. If not, please restart ES and OS and try again. Let me know if it works |
If I could help you, you can use the RATE button. Thank you. |
|
5/12/2016 7:09 AM | |
Joined: 3/14/2008 Last visit: 8/3/2024 Posts: 2079 Rating: (931)
|
Goodmorning amyLow, Please see below an extensive list of solutions that may cause your problem. You should check them: Problem:
To solve the problem you should check following points in sequence:
Computer names in the WinCC project are changed during download to match the designated station.Check if the Windows user is member in the correct User Groups!
ATTENTION: Disabeling of DEP may lead to increased vulnerabelity against injection of malicious code!
If you still have this behavior after you tried these steps, please contact the hotline. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
5/12/2016 10:59 AM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating: (31) |
Hi amyLow, if the copied thread from Oreca (original Thread ) does not help,
Regards |
12/27/2016 11:03 PM | |
Joined: 9/1/2005 Last visit: 8/1/2024 Posts: 4104 Rating: (194) |
New question published by Dazzycutter is split to a separate thread with the subject PCS7 download failure from ES to OS - could not be copied or could only be copied partially. Best regards |
My Forum is the place to personalize your profile, |
|
8/2/2024 1:25 PM | |
Joined: 7/30/2024 Last visit: 8/2/2024 Posts: 36 Rating: (0) |
New question published by Anhui14 is split to a separate thread with the subject problem with OS because of licenses . Best regards |
Follow us on