Industry Online Support
Technical Forum
8/3/2024 7:36 PM | |
Joined: 4/6/2018 Last visit: 8/3/2024 Posts: 15 Rating:
|
Hi, Hope you guys doing well! I am new to this guys, so apologies for being nube. I have to communicate S7 300 CPU 317-2PN/DP with Lexium 32m via Profibus (VW3A3607). So far I can read data from Lexium 32 to S7 -300 and can write parameters of servo drive from s7-300 as well but unable to change operating mode and run motor from s7-300. it shows in SoMove software "_WarnLatched Bit 21" = "HIGH" when I convert to fieldbus mode. THis warning related to fieldbus module. In this I have used Lexium Drive Profile 2 but earlier I have tried Lexium Drive Profile 1 and I have also tries PLCOpen Library but wont worked for me. What I think is that the issue which not change operating mode and run is the "_WarnLatched Bit 21" = "HIGH" but please guide me if i am wrong. Kindly guide me! AttachmentLXM32M S7300 Issue.zip (0 Downloads) |
Follow us on