9/10/2024 10:13 AM | |
Joined: 2/17/2020 Last visit: 9/10/2024 Posts: 1056 Rating:
|
Hi, The function rights specify which functions a user or a user group may use in a specific role. You can link different function rights to multiple roles. You can also add user-specific runtime rights. In the following example, you set up a user management for different users. SIMATIC HMI WinCC Unified V19 - Example: Setup of the local user management So, in your case, if the user-defined right "Test" is assigned to a role, and the logged in user does not have this role assigned, then he will not be able to press the protected button. |
A rating will be well appreciated. |
|
9/10/2024 11:14 AM | |
Joined: 2/17/2020 Last visit: 9/10/2024 Posts: 1056 Rating:
|
Exactly. I just saw that there is also an example that specifically talks about the configuration you are looking for to protect the button with a user-defined right: Example: Configuring a button with access protection Hope that helps! |
A rating will be well appreciated. |
|
Follow us on