(1)| 12/17/2024 3:31 PM | |
|
Joined: 5/6/2022 Last visit: 11/27/2025 Posts: 589 Rating:
|
Hi AutoGen_4884638, This alert was introduced in TIA V14 to educate people on network security. If you follow the link stated in the warning more information can be found there: https://www.siemens.com/industrial-security The purpose of this screen is to allow you to assign an IP address you want directly to your computer. For this reason this message is displayed so that you are aware of the security risks because the network can be changed. As for the upload problem, maybe the problem is that when you uploaded the project, the physical plc had a higher firmware that did not arrive with the software version with which you uploaded. Additionally, I attach an upload FAQ that may help you: "What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?" Best regards!
|
|
If this Information really helps, you could use the Rate function |
|
| 1/8/2025 8:08 AM | |
|
Joined: 11/23/2024 Last visit: 3/7/2025 Posts: 6 Rating:
|
I followed the steps and it didn't work, I don't know what to do anymore, now I get this error in the photo |
| 1/10/2025 8:40 AM | |
|
Joined: 4/24/2006 Last visit: 12/24/2025 Posts: 9097 Rating:
|
Hello, Please install the Hardware Support Packages for TIA Portal v15.1 Support Packages for the hardware catalog in the TIA Portal (HSP) (Are you sure you can not select Firmware 4.2, because in TIA Portal v14 it is possible, the HSP is for Firmware 4.3) Best regards, Wizard |
| 2/13/2025 4:37 PM | |
|
Joined: 2/13/2025 Last visit: 11/6/2025 Posts: 6 Rating:
|
Hi AutoGen : you must be select new and match hard ware form device explorer Tai portal and try again |
Follow us on