11/9/2021 10:14 AM | |
Joined: 3/3/2021 Last visit: 11/12/2024 Posts: 271 Rating:
|
Hello N_C_T, I have never seen such messages. Maybe the Siemens Support knows more about it. Best Regards, Fred |
6/6/2025 10:07 AM | |
Joined: 1/21/2013 Last visit: 9/15/2025 Posts: 4110 Rating:
|
Hi Mateusz, You're right; a WinCC Unified Basic Panel shouldn't have collaboration. However, it shouldn't trigger a Distribution Manager error either. Updating to the latest version may resolve this issue. Note that even if you're not using V20 for engineering, you can use the V20 Update 2 image, which is currently the latest version. Kind regards |
6/9/2025 3:03 PM | |
Joined: 1/21/2013 Last visit: 9/15/2025 Posts: 4110 Rating:
|
Hi F.Medeiros,
However, you may have to wait a long time for the engineers to find and solve an issue by luck alone. You can speed up the process by reporting the problem to Siemens by creating a support request. Kind regards |
7/25/2025 6:15 PM | |
Joined: 6/21/2020 Last visit: 8/13/2025 Posts: 12 Rating:
|
I created a support request and got in return the quote below. But to me it makes no sense, because I have the time set correctly in my Unified Basic Panel and S7-1500 PLC, and Basic panels do not support collaboration... And when I download to PLC and HMI, certificates are supposedly automatically downloaded.
|
Follow us on