(0)| 8/3/2025 6:07 AM | |
|
Joined: 3/14/2019 Last visit: 11/26/2025 Posts: 2 Rating:
|
Dear S7 400 CPU not Support OPC UA, If you want data to OPC you can add S71200 to ET200SP CPU as OPC Gateway. Thank |
| 8/7/2025 7:41 AM | |
|
Joined: 8/3/2009 Last visit: 12/19/2025 Posts: 16612 Rating:
|
Hello AutoGen_bd808 If you want to communicate between two S7-400 PLCs there are other ways than OPC. S7300/400 do not support OPC UA direcly on the PLC such as a S71200/1500. you can use a SIMATIC Net OPC Server for accessing the PLCs but the communication between the OPC Server and the PLC runs via S7protocol: https://support.industry.siemens.com/cs/ww/en/view/67295801 If you give us a few more information about your usecase and your requirments perhaps there are other ways to do it... Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on