8/5/2025 12:35 PM | |
Joined: 1/21/2013 Last visit: 9/18/2025 Posts: 4111 Rating:
|
Hi owenjpayne, First, determine why the PLC goes into STOP mode. The Unified System will not stop the PLC because of a communication error. It's possible that data corruption in the safety program was caused by the connection between the HMI and the PLC. Another possibility is that the HMI is setting the operating state, but this is only done intentionally. Kind regards |
Follow us on