8/18/2025 8:01 AM | |
Joined: 10/1/2015 Last visit: 9/4/2025 Posts: 22 Rating:
|
Yes, i have all the updates. Win 11 pro 24H2 Step7 5.7. SP3 Wincc V8.1.3 |
9/12/2025 11:25 AM | |
Joined: 11/1/2012 Last visit: 9/17/2025 Posts: 1 Rating:
|
Hello, did you solved it? I have same problem. Thanks |
9/17/2025 12:49 PM | |
Joined: 8/3/2009 Last visit: 9/22/2025 Posts: 16462 Rating:
|
Hello djpiky for compatibility of WinCC V8. with Step7 V5.7 Sp3 it is listed that you also have to use at least the Upd1 for V5.7 Sp3: https://support.industry.siemens.com/cs/de/en/view/109976902 Check if you have installed it and if not have a try Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on