9/17/2025 1:10 PM | |
Joined: 8/3/2009 Last visit: 9/23/2025 Posts: 16473 Rating:
|
Hello alamir-d The Installation of WinCC telecontrol V7.5 is a seperate DVD/ISO and is about over 300MB of data, so the Upd1 in this link is only a few MB of size, so I think this cannot be the whole installation and you would need the base software. In this delivery release are also the order numbers for the license and in this packages the base SW is integraded: https://support.industry.siemens.com/cs/de/en/view/109814522 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
9/22/2025 8:05 PM | |
Joined: 11/18/2017 Last visit: 9/22/2025 Posts: 3 Rating:
|
Hi Murof Thanks for your attention and response. You solved my problem. Best wishes
|
Follow us on