(0)| 10/28/2009 1:24 AM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi TechSal, Please follow the instructions attached, they may help. When you have correctly set up your PG/PC routing, you can communicate via your USB interface at 1.5MB over the 6MB connection between the two other objects. The reasons for Starter not connecting can be a pain, communication settings have to be correct, you have to have the same firmware version in the offline project as appears on the CF card. You can attach an archive of the project if you wish, we can then analyse your connection issues more closely. Regards, Graeme
AttachmentNote on using USB PC Adapter.pdf (658 Downloads) |
Follow us on