11/4/2010 7:07 PM | |
Joined: 9/27/2006 Last visit: 11/16/2024 Posts: 12294 Rating: (2691)
|
Hello deepak; Most of the infdormation you are looking for is available in the following manual: SIMATIC Fault-tolerant systems S7-400H -technical data of the CPU 412-3H: Chapter 17 -details on how to connect the CPUs together:Ch 3.3, p. 29: The basic S7-400H system, sections on Synchronization modules and Fiber optic cables. -power supply redudndancy: Chapter 3.3, p. 28and the following links: http://support.automation.siemens.com/WW/view/en/23431421 or Parallel connection of same type of power supplies for redundant operation -I/O redundancy, chapter 10, also Redundant I/Os with S7-400H systems -Fieldbus redundancy: chapter 7 (Profibus-DP) and Chapter 11 (Communictaions) Also look at the attached document on Y-Link for connection of non-redundant Profibus slaves to S7-400H redundant Profibus masters. Hope this helps, Daniel Chartier AttachmentY_LINK_E.pdf (238 Downloads) |
This contribution was helpful to1 thankful Users |
11/5/2010 4:18 AM | |
Posts: 65 Rating: (0) |
thanks for the help sir. |
Follow us on