11/11/2010 8:07 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating:
|
Hello, Look at How is the Y link structured? and What can you do if required modules are missing in the module catalog of the STEP 7 hardware configuration? More info for Y-Link you could find at this thread BR, Hristo Mihalev |
11/11/2010 8:36 AM | |
Joined: 10/7/2005 Last visit: 9/10/2024 Posts: 3020 Rating:
|
Hello Grim Reaper I'm afraid to say that there is no such thing asa single GSD file for the Y-Link. Owing to the nature of a Y-Link (which essentially "encapsulates" itsunderlyingDP Slaves and their I/O's) you must "create"your own GSD file for it and the tool to do so can be found HERE. Having said that, you would normally only do so with non S7DP Masters. Since you use PCS7I wonder why do you want to do a GSD based file configuration of the Y-Link? I hope this helps |
Cheers |
|
Follow us on