11/25/2006 2:21 PM | |
Posts: 4 Rating: (0) |
While connecting a TTL encoder with 5 V supply I cannot get any reaction at the inputs I0.3, I0.4, I0.5. Does anyone have a wiring diagram? |
11/27/2006 1:45 AM | |
Posts: 8 Rating: (0) |
The input specs state a logic 1 >15V at 2.5mA and logic 0 <5V at 1mA. You could use fast opto-isolators between PLC and encoder. Billy |
11/27/2006 8:28 AM | |
Posts: 2930 Rating: (432) |
Hi Toxic, Only a S7-200 PLC224XP supports 5V inputs and outputs. All the other PLC's has 24V inputs. I hope this helps. Reagrds Helmut |
Follow us on