3/26/2011 7:54 PM | |
Joined: 3/21/2006 Last visit: 10/1/2024 Posts: 10229 Rating: (1181) |
Hello Youcef, I suggest you to contact immediately with Siemens rep. in order eventually to repair it. You could use instead build in MPI port - 6ES7972-0CB20-0XA0 Best regards, Hristo Mihalev |
5/25/2011 9:28 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi you can use this usb-mpi adaptor regards ram |
5/25/2011 5:48 PM | |
Posts: 947 Rating: (45) |
Hello Possible burned out the power supply galvanically isolated Profibus transceivers in CP5611 (or similar). |
5/25/2011 7:29 PM | |
Posts: 691 Rating: (37) |
Have you checked CP5611 (Auto) rather than CP5611 (MPI) It might be that somenone changed the settings of Baud rate or Local Address |
5/27/2011 5:33 PM | |
Posts: 947 Rating: (45) |
Hello There are also devices RS232-MPI, Ethernet-MPI (profibus) |
Follow us on