Industry Online Support
Technical Forum
2/22/2012 3:44 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Hello, Let's start with - the hardware is the same. Just each version of PCS7 has own hardware released. In hardware configuration there exist a "PCS7" hardware profile regards installed version of PCS7 software. And yes, you can use a hardware from Standart hardware profile but - take a look at PCS7 Hardware Compatibility . Best regards, Hristo Mihalev |
2/23/2012 8:41 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi What UMENCHO said is right, you can use only High feature cards with PCS 7 system. That is the card will have channel and module diagnostics. You will have to refer the manual that is release modules for PCS7 V8.0 , Please see attchement. Your software part is little diffrent when compared to PLC part. Say for an eg CFC, SFC and the PCS7 block libary come as default with builtin block for applications. Have fun... AttachmentPCS7V8.0_Released_Moduels.pdf (211 Downloads) |
Jazz |
|
Follow us on