4/21/2012 8:29 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Dear Lucky123, Pleas euse Simatic H Station in this Case. |
VANDE MATARAM..... |
|
4/21/2012 8:31 AM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating: (1365) |
Hello , Please check the following thread for a sample configuration: F-System (S7-400F/FH) Simulation6.zip Best regards, Hamid Hosseini |
Last edited by: hdhosseini at: 4/21/2012 8:32 AM |
|
This contribution was helpful to1 thankful Users |
4/21/2012 9:51 AM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating: (1365) |
Hello Lucky123, H platform, is a special set up for high available configuration.You need several hardware component to set up a working H configuration. To program the H station, you program it as usual. But, there are some extra interfaces from OS of CPU available to diagnose(OB72). As you will read the manual for H CPUs for more information (which is necessary),you can find information on how to download or other PG operation (2 CPU exist master-standby). I strongly recommend you to read the H manual. SIMATIC High-availability systems S7-400H Best regards, Hamid Hosseini |
Last edited by: hdhosseini at: 4/21/2012 9:54 AM |
|
This contribution was helpful to1 thankful Users |
4/21/2012 10:13 AM | |
Posts: 947 Rating: (45) |
hi. Lucky123 You can use H-cpu in solo mode without syncromodul. but some function simple simatic 400 station (such a slave on profibus) in this case not possible. But with solo H-cpu you can make fault-tolerant connection, with simple simatic 400 stationthis not possible. After power on H-CPU make full test internal RAM (if backup battery fault or first start) min ~14min, simple simatic 400 station start much faster. in work h-cpu makt periodical own test For full configuration H-system need minimum 2cpu, 4 syncromodul, 2 fiberoptic cable, 2 power unit PS-40x and rack ur2-h or 2rack ur1 (ur2). With step 7 5.4sp5 you can use h-cpu version 4.5 |
Last edited by: gre_m at: 4/21/2012 10:16 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on