4/24/2012 2:25 PM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22687 Rating:
|
Hello, which S120 do you use? What interface is X46? Regards Christoph |
4/24/2012 3:58 PM | |
Posts: 8 Rating:
|
i'm using6SL3320-1TE32-1AA3, and X46 is configured to give me in a certain moment of my process a signal output to atctivate the brake of the motor. |
4/24/2012 8:08 PM | |
Posts: 8 Rating:
|
Hello ChristophD, Thanks for your help, i find a way to test the connector X46 using the Siemens SCOUT, using a parameter that always activate the brake, with the help of a miltimeter in tension scale, in the output of the connector (1,2 pins) was to have 24 VDC, but mine only have 2 VDC. So i isolate the problem. Thanks.
|
Follow us on