5/17/2012 1:30 PM | |||||||||||
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
|
||||||||||
Last edited by: UMENCHO at: 5/17/2012 1:33 PM |
|||||||||||
This contribution was helpful to1 thankful Users |
5/17/2012 2:12 PM | |
Joined: 8/18/2009 Last visit: 6/17/2024 Posts: 548 Rating: (33) |
DearUMENCHO, thanks for reply.... diff. between this two is only in power supply AC/DC ....right... also I have checked inSIMATIC PCS 7 AS Redundancy Stationconfigurator but there this PLC is not available also cant avoid CP443... from where are you select this bundle...Please tell me |
Last edited by: RAJKIRAN at: 5/17/2012 2:17 PMRajkiran Patil |
|
5/17/2012 2:42 PM | |
Joined: 8/18/2009 Last visit: 6/17/2024 Posts: 548 Rating: (33) |
DearUMENCHO you are not given answer of above question ...
|
Rajkiran Patil |
|
5/17/2012 2:59 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
In order to have it needs update 1 for PCS7 8.0 About CPs I can not answer you as I don't have experience. Try itSupport Request Best regards, Hristo Mihalev
|
5/18/2012 7:51 PM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating: (306)
|
HelloRAJKIRAN, Unfortunately, untilthismomentthere's no S7 bundle for 412-5H that has CP443-1. Let me highlight two things. 1- The 412-5H CPU has PN port that can do the job of the CP443-1. 2- The delivery of CP443-1 is frozen Best regards, H-H
|
5/18/2012 10:01 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
OK, this is my point of view. In order to close the thread should knoiw the RAJKIRAN's idea. Best regards, Hristo Mihalev
|
This contribution was helpful to2 thankful Users |
Follow us on