Industry Online Support
Technical Forum
1/14/2013 9:11 PM | |
Joined: 9/27/2006 Last visit: 11/16/2024 Posts: 12294 Rating: (2691)
|
Hello shailesh; Please read the following FAQ, and remember that forcing is a test function in Step 7: No switching to Redundant mode when PG function for Test and Startup is running in STEP 7 V5.x I think it is not difficult to deduce that other redundancy functionscould bedisabled while test functions are active. Try the switchoveragain while no forcing is enabled, see if the system responds. Hope this helps, Daniel Chartiier |
This contribution was helpful to1 thankful Users |
Follow us on