2/9/2010 7:35 AM | |
Posts: 3609 Rating:
|
Import of a Technical Question of an User Guest wrote: dear mr or mis please email a sample program og fm 350_2 with ladder for cpu 315-2dp best regards, |
2/13/2010 10:20 PM | |
Joined: 7/16/2006 Last visit: 1/2/2024 Posts: 1502 Rating:
|
Hi Please download this needing Software. http://support.automation.siemens.com/WW/view/en/28291262 After install, aditional examples for the FM350 are on your PC. |
Karl |
|
7/20/2013 5:27 PM | |
Joined: 9/27/2006 Last visit: 9/22/2025 Posts: 12420 Rating:
|
Hello Rufino; If you enter the Product Support pages, you use the Navigation tree to locate the correct module and find manuals, Updates, FAQs. See the attached screencapture. I have taken the liberty of uploading the correct linkfor these files. Hope this helps, Daniel Chartier |
8/13/2013 7:30 AM | |
Posts: 3 Rating:
|
Thank you for the answer. I will check it. |
8/13/2013 7:32 AM | |
Posts: 3 Rating:
|
I did it, I appreciate your help Best regards |
This contribution was helpful to
1 thankful Users |
1/3/2014 12:05 PM | |
Joined: 9/1/2005 Last visit: 9/19/2025 Posts: 4114 Rating:
|
follow up question published by binhsacomis split to a seperate thread with the subject module Fm350 call fc0 for HSC countervalue reset to 0 after power on Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
1/3/2014 3:45 PM | |
Joined: 6/24/2013 Last visit: 9/18/2025 Posts: 1696 Rating:
|
Hi Sample function attached as .AWL. You need add symbol FB200 and put Siemens FM350-2 FCs in project. FM350-2 is set to continuous counting and function is designed to convert reading to engineering units via a factor. moreover, homing [encoder clear on limit] is programmed as well. Hope this helps AttachmentFM350_2_FB200.zip (611 Downloads) |
Follow us on