(0)| 9/11/2007 12:09 PM | |
|
Posts: 51 Rating:
|
Depends from your application. MM430 supports all. http://support.automation.siemens.com/WW/view/de/6586565 http://support.automation.siemens.com/WW/view/de/10804923/133000 |
| 9/28/2007 1:23 AM | |
|
Posts: 112 Rating:
|
It is possible to read any parameter value from the drive. Parameters can be readas process data (PZD) or parameter access (PKW). The profiles set up certain amounts of PZD data and if you use PKW data,not the parameters that are read.The parameters that are read by PZD data can be changed by the various subparamters of parameter P2051. Parameters that are read by PKW data can be programmed in your PLC code and varied at runtime if necessary. Chapter 3.3 https://support.automation.siemens.com/WW/llisapi.dll?query=CB15&func=cslib.cssearch&content=skm%2Fmain.asp&lang=en&siteid=cseus&objaction=cssearch&searchinprim=0&nodeid0=10805386&x=26&y=9 |
Follow us on