3/19/2016 9:47 PM | |
Joined: 11/29/2011 Last visit: 10/24/2024 Posts: 1360 Rating: (232) |
Hi, Upload the entire Diagnostic buffer to see clearly what is happening. How is the ERROR-SEARCH mode completes? For detailed explanation check the SIMATIC Fault-tolerant systems S7-400H maual under chapter "11.3.6 ERROR-SEARCH mode". I would like to highlight something from this manual: "The purpose of ERROR-SEARCH mode is to find a faulty CPU. The standby CPU runs the full self-test, while the master CPU remains in RUN. If a hardware fault is detected, the CPU changes to DEFECTIVE state. If no fault is detected the CPU is linked up again. The faulttolerant system resumes the redundant system state. An automatic master-standby changeover then takes place. This ensures that when the next error is detected in errorsearch mode, the hardware of the previous master CPU is tested." So make sure you give enough time to this procedure to complete. |
Last edited by: MicroMan at: 3/19/2016 10:34:12 PM- What you read here, please check with manuals and your requirements. |
|
3/20/2016 1:28 PM | |
Joined: 1/19/2009 Last visit: 9/26/2018 Posts: 13 Rating: (0) |
Diagnostic Buffer after the end of error-search mode:
AttachmentDiagnose.txt (336 Downloads) |
Follow us on