Industry Online Support
Technical Forum
3/26/2008 8:28 PM | |
Posts: 5 Rating: (0) |
Hi, Here is my situation : Redundant Profibus-DP network linked to 2 417-4H Cpus, 4 racks for remote I/O (with double-head IM 153-2), and then 2 racks each composed with 2*IM 153-2 and Y-Coupler 197-1LB00-0XA0 to connect on each Y-Link 3 ABB Drives ACS800 which don't support redundancy. For software part I'm using PCS7 6.1 SP1. My problem is that up to now I didn't succeed to achieve my hardware configuration through step7 because i don't have corresponding GSD file. I read the ID contribution:26562190 and tried to use this tool but no result. I also read the documentation mentioned here : http://support.automation.siemens.com/WW/view/fr/1142696but nothing about gsd file... As i read in this topic, i downloaded the SP3 for step7 5.3 but no result. How can I insert and configure my Y-Coupler in step7 HW config ? Thanks a lot for your attention PS: I'm in commisioning in Turkey so I need your help asap |
Last edited by: CS Moderator at: 3/28/2008 12:47 AMnew subject after splitting Last edited by: Pavillon_Noir at: 3/26/2008 8:32 PM |
|
3/28/2008 12:50 AM | |
Joined: 9/1/2005 Last visit: 11/8/2024 Posts: 4111 Rating: (195) |
closed cause question posted twice. The second thread with the subject Y-Cooupler module in ET200M rack in PCS7 6.1 SP1is published within the conferenc Process Control Systems SIMATIC PCS 7. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on