7/18/2008 4:27 AM | |
Joined: 9/27/2006 Last visit: 9/16/2024 Posts: 12282 Rating: (2684) |
Hello redha; Are you sure about that part number? Siemens Mall only shows IM 153-1, IM 153-2 and Im 153-4: https://mall.automation.siemens.com/WW/guest/index.asp?aktPrim=-1&SearchIn=ALL&SearchFor=ARTICLE_NUMBER&SearchScrope=catalog&lang=en&searchText=IM+153-3 In any case, depending on your version of Step 7, the latest order numbers of the IM 153-x (for thew ET 200M slaves) should be in the Profibus Catalog of the HWConfig editor. And there are Internet updates available in case you don't have the latest and greatest version (uner Tools, Update catalog I believe). All configuration data for a Profibus-DP network is held in the master's memory, except for the individual Profibus address, which is loaded on each slave either with switches or through programming. Hope this helps, Daniel Chartier |
7/18/2008 6:24 AM | |
Joined: 9/27/2006 Last visit: 9/16/2024 Posts: 12282 Rating: (2684) |
Hello again redha; Look at Late's post in the following thread, reply no. 5 discusses the IM 153-3: /tf/WW/en/Posts/13582 It looks like this model was used for the S5 family, andearly redundancy packages for S7 PLCs. You will find a gsd file for this unit on the following link: http://support.automation.siemens.com/WW/view/en/113498 Hope this helps, Daniel Chartier |
7/24/2008 12:43 AM | |
Posts: 13 Rating: (0) |
hello what is meaning :ID d'événement 16# 2942 how i can know to use or download a new GSD in SIMATIC MANAGER What is the déference between IM153.3.ZIP and IM153-2FO -default.zip The GSD files are language dependent for configuration tools with extended configuration possibilities, i.e. COM PROFIBUS, STEP7 |
Follow us on