7/9/2018 11:52 PM | |
Joined: 11/12/2017 Last visit: 2/27/2024 Posts: 174 Rating:
|
Hello guys, If anybody has used the 1 count 24vdc/100kHz ET200s module. I have tried the sample program from Siemens but it doesn't seem to work. I have added the link below to the example. You can see my code is attached. I am trying to turn the output on when the count value reaches 2000 every time I turn the encoder the value goes to a max around 30 approx. then goes back to 0 (in both directions). I think the cause may be that when I monitor DB1.DBX13.0 (internal gate status) if seems to be flickering between high and low for some reason even though I have set it high in the code. My hardware config is also the same as the example and I have got the module working correctly with the first basic example in the attached link. Thanks for any replies, David https://support.industry.siemens.com/cs/at/en/view/87560033 |
Last edited by: Jen_Moderator at: 7/10/2018 12:22:07 PMOptimized link. |
|
Follow us on