8/29/2018 1:10 PM | |
Joined: 10/18/2012 Last visit: 12/15/2023 Posts: 225 Rating:
|
perhaps the system complains the restore disc, because the Field-PG is not in the correct boot-modus: BIOS / UEFI You can switch the boot-mode in BIOS-Setup from legacy (BIOS) to UEFI (UEFI) and vice versa. To enter the BIOS-Setup press ESC during system startup. Change the settings in the "Boot" submenu and save them by pressing the F10-key. Then try boot again from the restore disc. See also Field-PG manual, chapter 8.6 at https://support.industry.siemens.com/cs/ww/en/view/109482603 br, |
8/30/2018 1:44 PM | |
Posts: 53 Rating:
|
I changed from legacy to UEFI. With restoration CD inside, the windows won't start. It only shows me a screen "Resuming Windows" or "Opening Windows". But something happens as it lets me use external mouse connected to usb as well as keyboard and opens the external display. If I change to legacy, it will open the windows normally but I lose the mouse, keyboard and the display...
|
Follow us on