11/26/2018 3:43 PM | |
Joined: 9/16/2016 Last visit: 8/20/2024 Posts: 10 Rating: (0) |
Hello, I've a problem with a 416H cpu: the cpu is the rack#1 cpu in a H system. If I try to start the link-up and update operation the CPU turn into stop mode and requests a memory reset. The same behaviour if I try to download the project from Step7 (download to CPU1). I've done also a factory reset of the CPU but the situation is the same (see error buffer attached). If Install the cpu in a different rack with a complete different HW configuration the CPU is able to go in RUN mode, so I think that the problem is not the cpu but the HW config of the project. This config however has been compiled and verified without any problem in STEP7 so I have no idea where could be the issue. Any suggestion? AttachmentDiagnose_post aggiornamento fw.txt (337 Downloads) |
Follow us on