7/22/2019 10:24 AM | |
Joined: 7/18/2016 Last visit: 9/6/2021 Posts: 6 Rating:
|
Yes that is true, I have seen examples on the forum (as in the original post from D Chartier) where you can access the count value directly from the IO address. From the manual The Technology Objects (TO) of SIMATIC S7-1500(T) https://support.industry.siemens.com/cs/attachments/109743134/109743134_S7-1500T_TechnologyObjects_DOC_v10_en.pdf it looks like HSC is a TO. Also, when I add it in TIA it appears under Technology Objects. Where my understanding then falls short is what defines a TO, is it just the configuration or has it got something to do with a software object in the controller itself?
Attachment109743134_S7-1500T_TechnologyObjects_DOC_v10_en.pdf (322 Downloads) |
Last edited by: Jen_Moderator at: 07/22/2019 11:53:51Added file as an attachment. |
|
Follow us on