(0)| 10/2/2019 11:55 AM | |
|
Joined: 10/19/2016 Last visit: 10/7/2025 Posts: 12 Rating:
|
[snip] Do I need a new installation of Step7 Micro/WIN on this PC for the PC Access to retrieve all of the TAGs from the PLCs? As I've seen, I need the project to import the symbols to PC Access... This is a upgrade project and I just need to make the visualization, without the possibility to control/send data to PLC. Thank you! --------------------------------------------------------------------------- Split from: Connecting 4 S7-200 with an SCADA with read-only display and reporting |
Last edited by: sale_gr at: 10/02/2019 12:42:01Last edited by: The Helping Hand at: 10/02/2019 15:49:16Splitted follow up question. Last edited by: The Helping Hand at: 10/02/2019 15:54:28Added reference to original post. |
|
Follow us on