11/8/2008 7:44 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, In my opinion, teh IM153-3 is not available anymore (since 2001). See http://support.automation.siemens.com/WW/view/en/6447289 Redundant solutions use IM153-2 today. |
Last edited by: edr at: 11/8/2008 7:45 PMBest regards |
|
11/10/2008 4:58 AM | |
Joined: 9/27/2006 Last visit: 7/16/2024 Posts: 12268 Rating:
|
Hello Aym; Your description of the problem does not refer to redundancy, but to "Change module under operation" (Hotswap) functions. But this requires active bus modules in the IM 153-2 hardware, and the functions themselves are only supported by a S7-400 master, or a S7-300 Profibus module (CP 342-5); see the specifics here: http://support.automation.siemens.com/WW/view/en/186963 http://support.automation.siemens.com/WW/view/en/1826766 If you are using a CP 56xx as master, what do you plan to use as software/drivers behind it? You will have to handle the interrupt messages by yourself in this case. Hope this helps, Daniwel Chartier |
Follow us on