12/5/2008 9:37 AM | |
Posts: 13 Rating:
|
Hi J_Bell, I am using PCS7; V7.0, SP1; I have attached the complete diagnostic buffer of 2 CPUs n H system status, (time showed in diagnostic buffer 1994...., that i have to change yet) and anther thing, whnthe 1st CPU is stopped, the 2nd CPU taking control as master (there is indication MSTR ) , but actaully program is not running, whn the 1st CPU put on RUN, then only my program running, i see WINCC runtime, thanks in advance Sun AttachmentDiagnoseCPU1.pdf (309 Downloads) |
12/5/2008 9:38 AM | |
Posts: 13 Rating:
|
CPU2 diagnostic buffer
AttachmentDiagnoseCPU2.pdf (345 Downloads) |
12/5/2008 9:40 AM | |
Posts: 13 Rating:
|
My H system status in CPU run mode, AttachmentH system status.pdf (363 Downloads) |
Last edited by: sun1232 at: 12/5/2008 9:50 AM |
|
Follow us on